Ethernet Bootloader for MK64FX512 in Keil MDK5.21

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Bootloader for MK64FX512 in Keil MDK5.21

1,484 Views
haiwagnzuo
Contributor I

1、I have run Ethernet Bootloader on my board of MK64FX512 through IAR development;

2、But my company must use Keil MDK development,in In the process of transplantation,I Encountered one  problem.

  I want to put the Fapp_params to address 0x7f000 in flash,so I add the scatter file

  ER_m_fnet_app FappParams_start FappParams_size{
  fapp_params.o (+RO)
  }

bulid the project  the map file show

    Execution Region ER_m_fnet_app (Base: 0x0007f000, Size: 0x00000244, Max: 0x00000fff, ABSOLUTE)

    Base Addr    Size         Type   Attr      Idx    E Section Name        Object

    0x0007f000   0x0000008c   Code   RO         6026    i.fapp_params_from_flash  fapp_params.o
    0x0007f08c   0x000000dc   Code   RO         6027    i.fapp_params_to_flash  fapp_params.o
    0x0007f168   0x000000dc   Data   RO         6029    .fapp_params        fapp_params.o

it seems that the result is ok,

but I debug the project through the J-Link online,it come in hardfault at the beginning.I donot know what is wrong?

please help me ,thank you very much!

This is my scatter file

;#if (defined(__ram_vector_table__))
  #define __ram_vector_table_size__    0x00000400
;#else
  ;#define __ram_vector_table_size__    0x00000000
;#endif

#define m_interrupts_start             0x00000000
#define m_interrupts_size              0x00000400

#define m_flash_config_start           0x00000400
#define m_flash_config_size            0x00000010

#define m_text_start                   0x00000410
#define m_text_size                    0x0007EBF0

#define m_interrupts_ram_start         0x1FFF0000
#define m_interrupts_ram_size          __ram_vector_table_size__

#define m_data_start                   (m_interrupts_ram_start + m_interrupts_ram_size)
#define m_data_size                    (0x00010000 - m_interrupts_ram_size)

#define m_data_2_start                 0x20000000
#define m_data_2_size                  0x00020000

/* FNET application parameters (optional).*/
#define FappParams_start (0x0007FFFF + 1 - (4*0x400))
#define FappParams_end   0x0007FFFF
#define FappParams_size  0xFFF

/* Sizes */
#if (defined(__stack_size__))
  #define Stack_Size                   __stack_size__
#else
  #define Stack_Size                   0x01000
#endif

#if (defined(__heap_size__))
  #define Heap_Size                    __heap_size__
#else
  #define Heap_Size                    0x0400
#endif

LR_m_text m_interrupts_start m_text_start+m_text_size-m_interrupts_start { ; load region size_region
  VECTOR_ROM m_interrupts_start m_interrupts_size { ; load address = execution address
    * (RESET,+FIRST)
  }
  ER_m_flash_config m_flash_config_start FIXED m_flash_config_size { ; load address = execution address
    * (FlashConfig)
  }
  ER_m_text m_text_start m_text_size { ; load address = execution address
    * (InRoot$$Sections)
    .ANY (+RO)
  }
  ER_m_fnet_app FappParams_start FappParams_size{
  fapp_params.o (+RO)
  }

;#if (defined(__ram_vector_table__))
  VECTOR_RAM m_interrupts_ram_start EMPTY m_interrupts_ram_size {
  }
;#else
  ;VECTOR_RAM m_interrupts_start EMPTY 0 {
  ;}
;#endif
  RW_m_data m_data_start m_data_size { ; RW data
    .ANY (+RW +ZI)
  }
  RW_m_data_2 m_data_2_start m_data_2_size-Stack_Size-Heap_Size { ; RW data
    .ANY (+RW +ZI)
  }
  ARM_LIB_HEAP ((ImageLimit(RW_m_data_2) == m_data_2_start) ? m_data_2_start : +0) EMPTY Heap_Size { ; Heap region growing up
  }
  ARM_LIB_STACK m_data_2_start+m_data_2_size EMPTY -Stack_Size { ; Stack region growing down
  }
}

Labels (1)
0 Kudos
Reply
1 Reply

1,248 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi haiwagn zuo

According to your map file, Fapp_params is data (Read-Only). Could you clarify how this section gets value? also, if this variable is never initializaed, keil will try to initialize it to zero, which will cause a hardfault. If possible please check the use of UNINIT in keil.

Hope this helps.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply