Error in the BSDL file for the micro MK64FN1M0VMD12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error in the BSDL file for the micro MK64FN1M0VMD12

1,310 次查看
javmol
Contributor I

The BSDL file for the micro MK64FN1M0VMD12 I have downloaded from your web believe is inaccurate.

 

I'm doing a JTAG test and conflicts have certain signs, reviewing datasheet and

comparing the signal assignment with the pins see some errors. Also the ID is incorrect.

I reassigned the following signs and gotten my tests work properly.

 

Can you tell me if this file (K64_144bga.bsdl) there is a mistake or I need a different BSDL file?:

 

A greeting.

 

Changes PINOUT:

-H10: PTB0

-G10: PTB4

-E10: PTB16

-B10: N.C.

-A10: N.C.

-D10: PTB20

-J10: PTA27

-F10: PTB8

-M10: VSS

-L10: PTA14

-K10: PTA16

 

Changes ID:

attribute IDCODE_REGISTER of k60_1m: entity is

   "0001"  & -- Version

   

   "1011001101001010"  & -- Part Number

   

   "00000001110"  & -- Manufacturer Identity

   

   "1";  -- IEEE 1149.1 Requirement

Original Attachment has been moved to: K64_144bga_modified.bsdl.zip

0 项奖励
回复
2 回复数

1,105 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Javier,

First of all, thanks for your sharing.

I've attached the lastest BSDL file, please try again.

As you mentioned above, you had reassigned the incorrect pins in the BSDL file, and I was wondering if you can tell me what the exactly error of these pins are.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,105 次查看
rob1
Contributor I

I have to agree with Javier that there seems to be something wrong in the BSDL files on the website.  For example, with the K64 144 BGA BSDL file it says that port PTA14 is pin H10.  However, the datasheet says that PTA14 is on pin L10.

Thanks,

Rob

0 项奖励
回复