Error in SDK installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error in SDK installation

2,765件の閲覧回数
whiteliondd6
Contributor I

I am trying to install SDK for MKE16Z64VLD4 but, it is showing me error "Settings do not match for all tools". Give me solution how to solve this.

Capture.PNG

 

 

 

0 件の賞賛
返信
5 返答(返信)

2,754件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

When build SDK for MKE16Z64xxx4, did you select MCUXpresso IDE or ALL? I am able to install SDK_2_11_0_MKE16Z64xxx4 in MCUXpresso IDE v11.5.0.

Build SDK for MKE16Z64xxx4.pngMCUXpresso IDE v11.5.0 SDK_2_11_0_MKE16Z64xxx4.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,748件の閲覧回数
whiteliondd6
Contributor I

Hello

I am able to install it in MCUXpresso IDE but, I am facing an error while using config tools. I installed the SDK once again with the suggestion you gave and I selected all in toolchain option. Still, my error in not solved. 

When I opened pin configuration I got the error:

Capture.PNG

 

0 件の賞賛
返信

2,734件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Would you please screenshot the whole screen? Please tell me which SDK example to import to reproduce this problem. I test some example did not meet this issue.

0 件の賞賛
返信

2,706件の閲覧回数
whiteliondd6
Contributor I

I am trying to make new project in FRDM-KE16Z64VLD4 processor SDK. Then when I tried to use pin config tools at that time I faced this error, Here, I am sharing the snapshot.

Capture.PNG

 

0 件の賞賛
返信

2,700件の閲覧回数
ErichStyger
Specialist I

Hi @whiteliondd6 ,

is that project created/imported from the SDK (Quickstart Panel > New project) or did you modify it in any way? I see that you have KE15/KE16 projects in your workspace, so have you copied files between projects?

You can see what device is used here:

ErichStyger_0-1644988795432.png

These settings are stored in the .cproject file, while the Pins and Clocks settings are in the source files plus in the .mex file: so if you copy files from another device without the correct settings, you will get such a message.

If you created/imported an example from the SDK without touching it afterwards, then this would be an issue of the SDK itself.

And I think it would be helpful for the support team here if you could upload/post your project?

I hope this helps,

Erich

 

 

0 件の賞賛
返信