Error communicating to target processor TWR-K21D50M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error communicating to target processor TWR-K21D50M

2,275件の閲覧回数
v_snicarevs
Contributor III

Hi!

I have 5 TWR-K21D50M boards, 2 of the have following problems:

1.They wont program unless I use 'Mass erase on connect' and hold them in reset before starting programming.

2. While using sdk example (as GPIO one) it will program succesfully, but disconnect debugging in about 30 seconds.

3. When I am trieng to load a bigger binary I am getting error:

Loading programming algorithm ...

Done.

CMD>PM

Programming.

Processing Object File Data ...

Programmed.

Error communicating to target processor - try a RESET.

CMD>VC

Error loading CRC-16 algorithm.

Error loading CRC-16 Algorithm.

Error verifying flash of device

Error occured during Flash programming.

PE-ERROR: Error downloading to the device.

The other 3 boards work fine, all of them have the same version of firmware. I am using KDS. Debugging through onboard usb using P&E.

Any sugestion what could be wrong with them before I send them back to suplier?

Thank you!

ラベル(1)
タグ(1)
4 返答(返信)

2,076件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Viktors,

I have not seen these problems before, could you please try updating the firmware version of the Tower boards presenting the problem using the P&E Updater utility?

pastedImage_1.png

Also make sure that the jumper settings are in its default setting.

Another thing you could try is to install the latest P&E drivers, these can be downloaded from this page:

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Let me know if it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信

2,076件の閲覧回数
v_snicarevs
Contributor III

All the boards at firmware version 31.21 (also confirmed by P&E Firmware Information Utility).

Drivers are also recent.

The strangest thing is that 3 boards are absolutely fine, and working properly.

0 件の賞賛
返信

2,076件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Viktors,

This is strange, I would suggest you to contact your supplier.

Here is a link that might be helpful:

Returns and Warranty Information|NXP

Apologies for the inconvenience this may cause.

Best Regards!

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信

2,076件の閲覧回数
v_snicarevs
Contributor III

Thank you, our supplier has provided us replacement.