Erroneous interrupt generated when enabling LPTMR0 on FRDM-KL25Z board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Erroneous interrupt generated when enabling LPTMR0 on FRDM-KL25Z board

ソリューションへジャンプ
2,956件の閲覧回数
gustavod
Contributor III

Hi,

I´m trying to substitute my RTOS tick timer from the ARM systick to the LPTMR0 timer, in order to get better low power mode support.

However, when the code enables the LPTMR0 interrupt by the NVIC_ISER register, an erroneous interrupt is generated. The code that do that is:

NVIC_ISER |= NVIC_EN0_INT28; (on CoIDE)

or

  /* Common initialization of the CPU registers */    (on CodeWarrior 10.4)

  /* NVIC_ISER: SETENA|=0x10000000 */

  NVIC_ISER |= NVIC_ISER_SETENA(0x10000000);

The interrupt is generated as soon the LPTMR0 bit is set in NVIC_ISER register. The code that follows that lines is:

/* NVIC_IPR7: PRI_28=0xC0 */

NVIC_IPR7 = (uint32_t)((NVIC_IPR7 & (uint32_t)~(uint32_t)(

           NVIC_IP_PRI_28(0x3F)

          )) | (uint32_t)(

           NVIC_IP_PRI_28(0xC0)

          ));

/* SIM_SCGC5: LPTMR=1 */

SIM_SCGC5 |= SIM_SCGC5_LPTMR_MASK;

/* LPTMR0_CSR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,TCF=0,TIE=0,TPS=0,TPP=0,TFC=0,TMS=0,TEN=0 */

LPTMR0_CSR = LPTMR_CSR_TPS(0x00);

/* LPTMR0_CMR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,COMPARE=0 */

LPTMR0_CMR = LPTMR_CMR_COMPARE(module);

/* LPTMR0_CSR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,TCF=1,TIE=1,TPS=0,TPP=0,TFC=0,TMS=0,TEN=0 */

LPTMR0_CSR = (LPTMR_CSR_TCF_MASK | LPTMR_CSR_TIE_MASK | LPTMR_CSR_TPS(0x00));

/* LPTMR0_PSR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,PRESCALE=0,PBYP=1,PCS=1 */

LPTMR0_PSR = LPTMR_PSR_PRESCALE(0x00) |

             LPTMR_PSR_PBYP_MASK |

             LPTMR_PSR_PCS(0x01);

/* LPTMR0_CSR: TCF=0,TEN=1 */

LPTMR0_CSR = (uint32_t)((LPTMR0_CSR & (uint32_t)~(uint32_t)(

              LPTMR_CSR_TCF_MASK

             )) | (uint32_t)(

              LPTMR_CSR_TEN_MASK

             ));

The problem is that I do not want the interruption to be generated before the system starts. Why this interrupt is being generated even before the LPTMR0 clock is enabled?

Any help will be appreciated.

Best regards,

Gustavo

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,434件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Have you also tried to set the ICPR register before writing to ISER? This is used to avoid some unexcepted interrupt .

Please kindly refer to the following example for referenece.

void enable_irq (int irq)

{  

    /* Make sure that the IRQ is an allowable number. Up to 32 is

     * used.

     *

     * NOTE: If you are using the interrupt definitions from the header

     * file, you MUST SUBTRACT 16!!!

     */

    if (irq > 32)

        printf("\nERR! Invalid IRQ value passed to enable irq function!\n");

    else

    {

      /* Set the ICPR and ISER registers accordingly */

      NVIC_ICPR |= 1 << (irq%32);

      NVIC_ISER |= 1 << (irq%32);

    }

}


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,435件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Have you also tried to set the ICPR register before writing to ISER? This is used to avoid some unexcepted interrupt .

Please kindly refer to the following example for referenece.

void enable_irq (int irq)

{  

    /* Make sure that the IRQ is an allowable number. Up to 32 is

     * used.

     *

     * NOTE: If you are using the interrupt definitions from the header

     * file, you MUST SUBTRACT 16!!!

     */

    if (irq > 32)

        printf("\nERR! Invalid IRQ value passed to enable irq function!\n");

    else

    {

      /* Set the ICPR and ISER registers accordingly */

      NVIC_ICPR |= 1 << (irq%32);

      NVIC_ISER |= 1 << (irq%32);

    }

}


0 件の賞賛
返信
2,434件の閲覧回数
gustavod
Contributor III

Hi Kan,

Thank you for remember me that. I completely forgot that there is a register to clear pending interrupts.

The code you posted solved the problem.

Best regards,

Gustavo

0 件の賞賛
返信