Erroneous Tamper event

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Erroneous Tamper event

10,631 Views
PHXFAE
Contributor II

I have a customer who is the MK21 and is utilizing the tamper detect features.  He is finding the he is getting false tamper event detections when he has a lose USB connection. The tamper detect registered is the clock., RTC he's assuming.  He's removed the check for this tamper event and right now everything is stable.  Can we get a little more information on this tamper event and why it seems like a bad USB connection could cause a false tamper event?

Thx for the help.

Labels (1)
0 Kudos
Reply
12 Replies

10,181 Views
PHXFAE
Contributor II

The part that the customer is using is this, MK21DN512VMC5.Not sure how to figure out the mask set.

0 Kudos
Reply

10,181 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

The mask set is on the surface of the device, right below the part number, and it is related with the silicon revision, so having it would be helpful to locate the cause. Please kindly refer to the following for details.

The snapshot shot is from TWR-K21D50M, and the device on that board has the 0n89e mask set.

Untitled.png


Have a great day,
Kan

0 Kudos
Reply

10,181 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

I just got the feedback from our AE team,and they think it is mostly caused by voltage change on VBAT. They suspected USB connection is causing VBAT change. Please kindly ask your customer to check this and let him send us the PCB layout file and schematics.

BTW, May I have more information about your customer? Thanks!


Have a great day,
Kan

0 Kudos
Reply

10,170 Views
PHXFAE
Contributor II

Hi Kan,

For some reason I can’t upload this on the community site so hopefully you can get it here. I do not have the mask set yet. Hopefully, I will get that soon. However, I do have his design files (attached).

Thx, Alex

0 Kudos
Reply

10,170 Views
cutworth
NXP Employee
NXP Employee

Hi Alex,

Could you provide your email address? I need more information to help on this.

Hao

0 Kudos
Reply

10,170 Views
PHXFAE
Contributor II
0 Kudos
Reply

10,170 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

Thanks for the information! I have forwarded this to our Apps team, and will let you know when I have any more information!

Thanks for your patience!


Have a great day,
Kan

0 Kudos
Reply

10,170 Views
PHXFAE
Contributor II

Can I get someone to look at this issue.  It seems to have gone dormant.

Thx

0 Kudos
Reply

10,170 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Sorry Alex! I was in a training last week. Would you please give me the full part number and the mask set of the MK21 that you mentioned? I will check with the IP Owner for this issue. Thanks for your patience!


Have a great day,
Kan

0 Kudos
Reply

10,170 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Kan_Li please continue with the follow up.

0 Kudos
Reply

10,170 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

Did the issue happen when you remove MK21 from PC host? How about the PCB layout? is the clock path put closely to the USB bus? Please kindly help to clarify.


Have a great day,
Kan

0 Kudos
Reply

10,170 Views
PHXFAE
Contributor II

If you wiggle the USB cable, with a bad cable, it produces bad connections and thru that the tamper seems to trip. The RTC clock path is REALLY close to the chip and the same is with the OSC.

0 Kudos
Reply