Erasing with FlashEraseSector(... )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Erasing with FlashEraseSector(... )

跳至解决方案
2,560 次查看
pietrodicastri
Senior Contributor II

Good morning

I try to erase using  the C90TFS/FTF FlashEraseSector().

When executing the code

 

REG_WRITE(pSSDConfig->ftfxRegBase + FTFx_SSD_FCCOB0_OFFSET, FTFx_ERASE_SECTOR);

 

in the body of the function I get a bus error.

The target hardware is a KvikStik.

I think many of You already have done.

 

Suggestions????

 

 

Thank Everybody

 

 

Please I just need a small chunck of time.. I added the project...

 

 

Thank You

Original Attachment has been moved to: TestFlash.zip

标签 (1)
标记 (2)
1 解答
2,097 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check attached project, which includes how to use Flash Erase Sector command [NormalDemo].
Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,098 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check attached project, which includes how to use Flash Erase Sector command [NormalDemo].
Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,097 次查看
pietrodicastri
Senior Contributor II

Thank You..

I am going to check, anyway I see a qualified example..

Thank You

0 项奖励
回复