Erasing with FlashEraseSector(... )

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Erasing with FlashEraseSector(... )

ソリューションへジャンプ
2,504件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I try to erase using  the C90TFS/FTF FlashEraseSector().

When executing the code

 

REG_WRITE(pSSDConfig->ftfxRegBase + FTFx_SSD_FCCOB0_OFFSET, FTFx_ERASE_SECTOR);

 

in the body of the function I get a bus error.

The target hardware is a KvikStik.

I think many of You already have done.

 

Suggestions????

 

 

Thank Everybody

 

 

Please I just need a small chunck of time.. I added the project...

 

 

Thank You

Original Attachment has been moved to: TestFlash.zip

ラベル(1)
タグ(2)
1 解決策
2,041件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check attached project, which includes how to use Flash Erase Sector command [NormalDemo].
Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,042件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check attached project, which includes how to use Flash Erase Sector command [NormalDemo].
Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,041件の閲覧回数
pietrodicastri
Senior Contributor II

Thank You..

I am going to check, anyway I see a qualified example..

Thank You

0 件の賞賛
返信