Enabling interrupt on a pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling interrupt on a pin

Jump to solution
9,632 Views
indraastra
Contributor II

Hi there,

I am a complete newbie to Freescale microcontrollers and the Freedom KL25Z development board, but I have watched all of Eli Hughes' excellent introductory videos. I'm trying to build on his examples by writing a simple program that toggles an LED on or off by watching for an interrupt on a pin driven by a simple pushbutton switch. I want to configure this pin to use the internal pullup resistor so that when the switch is pushed, the pin is pulled low; correspondingly, I want the interrupt to fire on a falling edge.

The code below outlines my basic approach to this, and I think I have enabled interrupts for both Port A Pin 20 (where the switch is connected) and also Port A on the NVIC. However, when I push the button, the code seems to exit immediately and I see the message "Suspended: Signal 'Halt' received..." from the CodeWarrior debug view. What am I doing wrong?

#include "derivative.h" /* include peripheral declarations */

int fired = 0;

void PORTA_IRQHandler() {

  fired = 1;

}

int main(void)

{

  SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK;

  PORTA_PCR20 = PORT_PCR_MUX(1) | PORT_PCR_IRQC(6) | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;  // Interrupt on falling edge.

  // enable IRQ on Port A, pin 20

  int irq_num = INT_PORTA - 16;

  NVIC_ICPR |= 1 << irq_num;

  NVIC_ISER |= 1 << irq_num;

  for (;;) {

       if (fired == 1) {

           // toggle LED

            fired = 0;

       }

  }

  return 0;

}

I have a breakpoint set within the ISR which is never reached.

0 Kudos
Reply
1 Solution
5,856 Views
indraastra
Contributor II

Looks like I had the misfortune of picking the RESET pin to test interrupts on! Switching to another pin on port A did the trick.

View solution in original post

0 Kudos
Reply
6 Replies
5,856 Views
cris
Contributor II

Hello everyone,

I am also trying to program an interrupt on a falling edge but with the Freedom KL05Z development board. I have followed the previous example and I have tried different pins but it's not working. I don't know what am I missing, in the reference manual of the KL05Z the configuration do not seem to be different...

Thank you in advance! :smileyhappy:   

0 Kudos
Reply
5,856 Views
mjbcswitzerland
Specialist V

Hi

Have you enabled the "global interrupt" as well as configuring the NVIC  and the port interrupt itself?

Regards

Mark

0 Kudos
Reply
5,856 Views
cris
Contributor II

Hi Mark,

I'm sorry, I am very new to Freescale microcontrollers and I don't know how to enable the global interrupt. I have been looking for it in the reference manual and this is in section 11.6.2. Global pin control: "However, the interrupt functions cannot be configured using the global pin control registers". I must be mistaking parameters...

Thank you for your time!

0 Kudos
Reply
5,856 Views
mjbcswitzerland
Specialist V

Cris

The global interrupt control is in the ARM procesor.

Using Codewarrior it can be enabled with asm("cpsie   i");

Regards

Mark

0 Kudos
Reply
5,856 Views
indraastra
Contributor II

Looks like I had the misfortune of picking the RESET pin to test interrupts on! Switching to another pin on port A did the trick.

0 Kudos
Reply
5,856 Views
indraastra
Contributor II

I see that I made a mistake and should have set PORT_PCR_IRQC(0xA) instead, but the code still terminates prematurely.

0 Kudos
Reply