Enable all TSI channels in low power mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable all TSI channels in low power mode

1,428件の閲覧回数
karthikbandi
Contributor I

Hello,

I am using MKL16Z MCU and i want to enable all channels in low power mode, but according to PE and reference manual its not possible to enable all channels to wake up the MCU, only one channel can be used. How i can configure to use all channels.

If its not possible to enable all channels, is there any other microcontroller which supports to enable all TSI channels in low power mode.

Thanks,

0 件の賞賛
返信
3 返答(返信)

1,289件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct that you can set & enable any of the TSI channels (0-15) but only one channel at a time.


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 件の賞賛
返信

1,289件の閲覧回数
karthikbandi
Contributor I

Hai

But in MK10DN64 microcontroller it says in VLPS mode all channels are in active mode.

I want o configure TSI  in normal active mode and VLPS modeTSI modes_MK10.PNG

0 件の賞賛
返信

1,289件の閲覧回数
karthikbandi
Contributor I

I found one MCU MK10DN64 where i can enable all channels of TSI in low power mode. Is it OK?

0 件の賞賛
返信