Electronical installation with Kinetic K82F board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Electronical installation with Kinetic K82F board

2,449件の閲覧回数
mesdouaabderraz
Contributor III

Hi nxp community,
I try to do an electronical installation in order to add an extreme interuption button.
But I can not find any examples on this,
I use Freedom Board for Kinetic K82F Hardware (FRDM-K82F) and a button as in the picture attached.

If anyone can help me by  suggesting  an example or a tutorial on the subject,

thank you.

0 件の賞賛
返信
3 返答(返信)

2,352件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

There is one example available about input interrupt. In order to get it, please go to https://mcuxpresso.nxp.com/en/builder where you can generate the SDK (Software Development Kit) for your specific board and IDE. Once you’ve already generated it, please import the corresponding project which is in the following path in your K82F’s SDK Folder:

SDK_2.2_FRDM-K82F.zip\boards\frdmk82f\driver_examples\gpio\input_interrupt

Regards,

Ivan.

0 件の賞賛
返信

2,352件の閲覧回数
mesdouaabderraz
Contributor III

please i look for a interrupt pin on frdm-k82f. 

0 件の賞賛
返信

2,352件の閲覧回数
mesdouaabderraz
Contributor III


Hello

Thank you for your reply,

But when I try to use the functions of the button sw2 on my project it does not work, I even made a test by copying the same program "gpio_input_interrupt_frdmk82f" in a new project, but the button do not work. I copied the "pine mux" too,

I think there is a file that I forgot.
Can you please tell me what are the steps to check when you copy an example project into a new project.

Regards,

Mesdoua.

0 件の賞賛
返信