ERROR: Can not read register 1 (R1) while CPU is running

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR: Can not read register 1 (R1) while CPU is running

6,423 Views
linwang-wei
Contributor I

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link OpenSDA 2 compiled Oct 13 2015 12:10:56

Hardware: V1.00

S/N: 621000000

Checking target voltage...

Target voltage: 3.30 V

Listening on TCP/IP port 2331

Connecting to target...Connected to target

Waiting for GDB connection...Connected to 127.0.0.1

Reading all registers

Read 4 bytes @ address 0x00000000 (Data = 0x20010000)

Target interface speed set to 1000 kHz

Resetting target

Halting target CPU...

...Target halted (PC = 0x000004D8)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 20010000, MSP= 20010000, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 000004D8

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Select auto target interface speed (1429 kHz)

Flash breakpoints enabled

Semi-hosting enabled (VectorAddr = 0x08)

Semihosting I/O set to TELNET Client

Downloading 1024 bytes @ address 0x00000000 - Verified OK

Downloading 16 bytes @ address 0x00000400 - Verified OK

Downloading 16160 bytes @ address 0x00000410 - Verified OK

Downloading 16224 bytes @ address 0x00004330 - Verified OK

Downloading 16368 bytes @ address 0x00008290 - Verified OK

Downloading 16368 bytes @ address 0x0000C280 - Verified OK

Downloading 16368 bytes @ address 0x00010270 - Verified OK

Downloading 16368 bytes @ address 0x00014260 - Verified OK

Downloading 16368 bytes @ address 0x00018250 - Verified OK

Downloading 16368 bytes @ address 0x0001C240 - Verified OK

Downloading 16368 bytes @ address 0x00020230 - Verified OK

Downloading 16368 bytes @ address 0x00024220 - Verified OK

Downloading 16368 bytes @ address 0x00028210 - Verified OK

Downloading 16368 bytes @ address 0x0002C200 - Verified OK

Downloading 16368 bytes @ address 0x000301F0 - Verified OK

Downloading 16368 bytes @ address 0x000341E0 - Verified OK

Downloading 16368 bytes @ address 0x000381D0 - Verified OK

Downloading 16368 bytes @ address 0x0003C1C0 - Verified OK

Downloading 2872 bytes @ address 0x000401B0 - Verified OK

Downloading 8 bytes @ address 0x00040CE8 - Verified OK

Downloading 4 bytes @ address 0x00040CF0 - Verified OK

Downloading 4 bytes @ address 0x00040CF4 - Verified OK

Downloading 144 bytes @ address 0x00040CF8 - Verified OK

Read 4 bytes @ address 0x000004D8 (Data = 0xF001B672)

Comparing flash   [....................] Done.

Erasing flash     [....................] Done.

Programming flash [....................] Done.

Verifying flash   [....................] Done.

Resetting target

Halting target CPU...

...Target halted (PC = 0x000004D8)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 20010000, MSP= 20010000, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 000004D8

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Read 4 bytes @ address 0x000004D8 (Data = 0xF001B672)

Starting target CPU...

ERROR: Can not read register 15 (R15) while CPU is running

...Target halted (PC = 0x00000000)

Reading all registers

ERROR: Can not read register 0 (R0) while CPU is running

ERROR: Can not read register 1 (R1) while CPU is running

ERROR: Can not read register 2 (R2) while CPU is running

ERROR: Can not read register 3 (R3) while CPU is running

ERROR: Can not read register 4 (R4) while CPU is running

ERROR: Can not read register 5 (R5) while CPU is running

ERROR: Can not read register 6 (R6) while CPU is running

ERROR: Can not read register 7 (R7) while CPU is running

ERROR: Can not read register 8 (R8) while CPU is running

ERROR: Can not read register 9 (R9) while CPU is running

ERROR: Can not read register 10 (R10) while CPU is running

ERROR: Can not read register 11 (R11) while CPU is running

ERROR: Can not read register 12 (R12) while CPU is running

ERROR: Can not read register 13 (R13) while CPU is running

ERROR: Can not read register 14 (R14) while CPU is running

ERROR: Can not read register 15 (R15) while CPU is running

ERROR: Can not read register 16 (XPSR) while CPU is running

ERROR: Can not read register 17 (MSP) while CPU is running

ERROR: Can not read register 18 (PSP) while CPU is running

ERROR: Can not read register 24 (PRIMASK) while CPU is running

ERROR: Can not read register 25 (BASEPRI) while CPU is running

ERROR: Can not read register 26 (FAULTMASK) while CPU is running

ERROR: Can not read register 27 (CONTROL) while CPU is running

ERROR: Can not read register 32 (FPSCR) while CPU is running

ERROR: Can not read register 33 (FPS0) while CPU is running

ERROR: Can not read register 34 (FPS1) while CPU is running

ERROR: Can not read register 35 (FPS2) while CPU is running

ERROR: Can not read register 36 (FPS3) while CPU is running

ERROR: Can not read register 37 (FPS4) while CPU is running

ERROR: Can not read register 38 (FPS5) while CPU is running

ERROR: Can not read register 39 (FPS6) while CPU is running

ERROR: Can not read register 40 (FPS7) while CPU is running

ERROR: Can not read register 41 (FPS8) while CPU is running

ERROR: Can not read register 42 (FPS9) while CPU is running

ERROR: Can not read register 43 (FPS10) while CPU is running

ERROR: Can not read register 44 (FPS11) while CPU is running

ERROR: Can not read register 45 (FPS12) while CPU is running

ERROR: Can not read register 46 (FPS13) while CPU is running

ERROR: Can not read register 47 (FPS14) while CPU is running

ERROR: Can not read register 48 (FPS15) while CPU is running

ERROR: Can not read register 49 (FPS16) while CPU is running

ERROR: Can not read register 50 (FPS17) while CPU is running

ERROR: Can not read register 51 (FPS18) while CPU is running

ERROR: Can not read register 52 (FPS19) while CPU is running

ERROR: Can not read register 53 (FPS20) while CPU is running

ERROR: Can not read register 54 (FPS21) while CPU is running

ERROR: Can not read register 55 (FPS22) while CPU is running

ERROR: Can not read register 56 (FPS23) while CPU is running

ERROR: Can not read register 57 (FPS24) while CPU is running

ERROR: Can not read register 58 (FPS25) while CPU is running

ERROR: Can not read register 59 (FPS26) while CPU is running

ERROR: Can not read register 60 (FPS27) while CPU is running

ERROR: Can not read register 61 (FPS28) while CPU is running

ERROR: Can not read register 62 (FPS29) while CPU is running

ERROR: Can not read register 63 (FPS30) while CPU is running

ERROR: Can not read register 64 (FPS31) while CPU is running

Read 4 bytes @ address 0x00000000 (Data = 0x20010000)

Read 4 bytes @ address 0x00000000 (Data = 0x20010000)

可以編譯,但是寫入時就出現這個,K22F無法正常運作

0 Kudos
Reply
1 Reply

2,771 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

The Fig 1 illustrates the normal connection between the OpenSDA Jlink and the FRDM-K22F120.

So I was wondering if you can tell me what the board you use.

2016-01-05_13-59-09.jpg
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply