ENET uDMA and Descriptors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ENET uDMA and Descriptors

Jump to solution
2,901 Views
matthewdowsett
Contributor I


Hi,

I am using the TWR-K60N512 and the TWR-SER modules. My project is a CAN to Ethernet bridge bare-metal system.

Using the drivers provided by Freescale I am reasonably sure I have the ENET configured correctly. Also can take a register dump from the PHY and the contents look OK cross checking with the KSZ8041 Datasheet. When I connect the provided Ethernet cable to my PC I get both green LEDs active, with one LED flashing each time my PC sends an Ethernet packet (I am spying using MS Network Monitor).

I have hard coded a TX packet and called enet_transmit_packet function. So both TDAR and RDAR are set but no TX or RX events are occurring. The RX and TX descriptor ring buffers are never altered as I expect they would be.

My question is does the uDMA need any consideration? I am running a very simple bare metal system that has not touched the AIPS, DMA, etc.

Or any other tips would be greatly appreciated :-)

Matthew

Labels (1)
0 Kudos
Reply
1 Solution
2,537 Views
matthewdowsett
Contributor I

Hi,

Problem solved - the issue was in the MCG setup - a clocking issue. It appears that the uDMA does not need any consideration other than clearing the MPU CESR VLD bit.

Matthew

View solution in original post

0 Kudos
Reply
2 Replies
2,537 Views
matthewdowsett
Contributor I

Hi,

Problem solved - the issue was in the MCG setup - a clocking issue. It appears that the uDMA does not need any consideration other than clearing the MPU CESR VLD bit.

Matthew

0 Kudos
Reply
2,537 Views
Monica
Senior Contributor III

Matthew,

that's great, thanks for sharing the workaround with us!

You rock!

Best,

Monica.

0 Kudos
Reply