EGUI 3.0 Button to work on click not release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EGUI 3.0 Button to work on click not release

1,663件の閲覧回数
tylerwebber
Contributor I

I recently upgraded to eGUI 3.0 and now notice that the buttons are going high on press release not on first press. I have enabled D4D_OBJECT_F_FASTTOUCH, but it still is waiting until the release of the button to go high.  Is there a setting that I am missing somewhere? Thanks for your help.

タグ(4)
0 件の賞賛
返信
1 返信

1,565件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Tyler,

For eGUI:

      Freescale eGUI: Graphical LCD Driver for MCUs|Freescale

I recommend you to use the link below:

      https://github.com/Gargy007/eGUI

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信