EEPROM emulation by using FLASH memory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEPROM emulation by using FLASH memory?

ソリューションへジャンプ
6,164件の閲覧回数
pengliang
Contributor III

Hi all,

Does anyone know how to use flash memory emulate EEPROM? if yes, could you provide sample code tutorial?

Thank you

0 件の賞賛
返信
1 解決策
3,653件の閲覧回数
apanecatl
Senior Contributor II

You can download our flash drivers for EEPROM emulation in Non Flex NVM memory for Kinetis and ColdFire devices:

TFS Flash Driver Software for Kinetis and ColdFire+ Microcontrollers

If you are looking for EEPROM emulation using Flex NVM memory check the following App Note:

http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,654件の閲覧回数
apanecatl
Senior Contributor II

You can download our flash drivers for EEPROM emulation in Non Flex NVM memory for Kinetis and ColdFire devices:

TFS Flash Driver Software for Kinetis and ColdFire+ Microcontrollers

If you are looking for EEPROM emulation using Flex NVM memory check the following App Note:

http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf

0 件の賞賛
返信
3,653件の閲覧回数
pengliang
Contributor III

Thank you for the information.

Does the driver support Kinetis L family? thank you

0 件の賞賛
返信
3,653件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Yes, you can even find an example in the installation folder of the C90TFS driver.

(Installation path)\Standard Software Driver vBeta033\C90TFS\Demos\L2K

3,653件の閲覧回数
apanecatl
Senior Contributor II

I'm not pretty sure however the flash routines should be identical, so most likely yes

0 件の賞賛
返信