EEPROM TWRkit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM TWRkit

2,291 Views
xavierbuhot
Contributor II

Hello,

I would like to use the eeprom on my k60 kinetis so I found the example supply with th TWRkit.

When I launch the program the EEPROM still lock and never ready, the program are still running at that sentence:

/* Wait for the command to complete */
while(!(FTFL_FCNFG & FTFL_FCNFG_EEERDY_MASK));

Can someone help me?

Best regard.

4 Replies

2,089 Views
xavierbuhot
Contributor II

I just notice that I get the TWR_K60N512 and there is not FLEXNVM memory, it is a devices with program flash only.

So I can use the flash to store all the data? How can I setup the flash part (at that range adress 0x1400_0000–0x17FF_FFFF) to b able to use it?

Is there any example?

0 Kudos
Reply

2,089 Views
xavierbuhot
Contributor II

More informations about my problem.

I try to put my program into RAM and try to write on flash blocks. But I still have Hard fault and vector 3 interrupt.

Is it really possible to write in flash memory?

Please ... :smileysad:

0 Kudos
Reply

2,089 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Xavier:

I noticed you submitted a Service Request about these questions. Are your doubts clarified?

Just to summarize:

- You are correct, K60N512 does not have Flex NVM. But yes, you can still use part of the program flash to store non volatile data.

- You cannot use range 0x1400_0000–0x17FF_FFFF, since this is not present in your  device.

- The available flash memory in K60N512 is from 0x00000000 to 0x0007FFFF.

- For Flash memory storage and code examples, you can refer to Freescale Standard Software Driver (C90TFS), downloadable from the next link:

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe

I hope this helps.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,089 Views
xavierbuhot
Contributor II

Hello,

Thank you for your attention.

I finally achieve to ake it work. In my message I made a mistake, I did

wrote in the right part of the memory (0x00000000 to 0x0007FFFF.) but I

forget to setup the configuration of the flash memory.

Thank you again.

Best regard.

2014-09-09 4:02 GMT+02:00 Jorge_Gonzalez <[email protected]>:

<https://community.freescale.com/>

EEPROM TWRkit

reply from Jorge_Gonzalez

<https://community.freescale.com/people/Jorge_Gonzalez?et=watches.email.thread>

in * Kinetis Microcontrollers* - View the full discussion

<https://community.freescale.com/message/433553?et=watches.email.thread#433553>