Dutycycle Update in MK60 using Flex timers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dutycycle Update in MK60 using Flex timers

ソリューションへジャンプ
1,931件の閲覧回数
mss
Contributor I


Hi,

I am using MK60 Flex times for pwm generation. I have the pwm going in the complemetary mode where the dutycycle is controlling the speed as well as the direction of dc motor. The motor runs fine but as soon as I update the dutycycle the motor stops. I can see that the registers C0V and C1V update with the new dutycycle values but at that point the motor stops. I am not sure why this is happening. Did anybody run across this issue or have any idea why this might be happening? Thanks much for the help.

SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;

SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;

PORTC_PCR1 = 0x400;

PORTC_PCR2 = 0x400;

GPIOA_PDDR |= (1 << 24);            

GPIOA_PDOR |= (1 << 24);

FTM0_MODE |= FTM_MODE_FTMEN_MASK;

FTM0_COMBINE = 0x32;

FTM0_DEADTIME = 0x46;

FTM0_MOD = 0x000012A;     /* PWM period */

FTM0_C0SC = 0x28;

FTM0_C0V =0x0ff;

FTM0_C1SC = 0x28;

FTM0_C1V =0x0ff;

FTM0_PWMLOAD = FTM_PWMLOAD_LDOK_MASK;

FTM0_SC = 0x08;

FTM0_SYNCONF = 0x00001FB4;

FTM0_SYNC = 0x80;

if (counter>2 & counter<=8){           // I have defined an infinite counter in the main loop.

FTM0_C0V =0x0EE;                                    <--------------Motor stops running here.

FTM0_C1V =0x0EE;                                    <--------------Motor stops running here.

FTM0_OUTMASK = 0xFF;

FTM0_SYNC = 0x88;  

FTM0_SWOCTRL = 0x3F3F;

FTM0_PWMLOAD = FTM_PWMLOAD_LDOK_MASK;

}






ラベル(1)
0 件の賞賛
返信
1 解決策
1,512件の閲覧回数
apanecatl
Senior Contributor II

You need to check when is the register being updated, depending on the mode the FTM is working, you can check it here in the CnV register update table (reference manual chapter 40.4.10.3):

2868_2868.png

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,513件の閲覧回数
apanecatl
Senior Contributor II

You need to check when is the register being updated, depending on the mode the FTM is working, you can check it here in the CnV register update table (reference manual chapter 40.4.10.3):

2868_2868.png

0 件の賞賛
返信