Driving a BLDC motor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driving a BLDC motor?

ソリューションへジャンプ
3,703件の閲覧回数
juanramonet
Contributor I

Hello, I am trying to figure out what are all the components that I need to drive a BLDC motor to speeds of 5-100 rpm. The motor has hall sensors. I am not familiar with brushless motors and circuitry so any help would be great! Are there any Freescale drivers that could be used?

0 件の賞賛
返信
1 解決策
3,436件の閲覧回数
fantasy
NXP Employee
NXP Employee

HI, juan

I'd like to suggest you can choose the KE02 , KE02 is a 5 V MCU with enhanced FlexTimer(FTM), suitable for BLDC motor control. You can learn more detail information about KE02 through the link as below.

http://cache.freescale.com/files/32bit/doc/ref_manual/MKE02Z64M20SF0RM.pdf?fasp=1&WT_TYPE=Reference%...

And there is a ready-made solution to diver BLDC with FRDM-KE02Z. You can learn more about the solution by click the link below.

http://cache.freescale.com/files/32bit/doc/app_note/AN4776.pdf?fromsite

Have a good day,

Xi Fan

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,436件の閲覧回数
fantasy
NXP Employee
NXP Employee

Hi,

Maybe you can refer to the simple code of KV10, it has three versions,CW,keil and IAR, and you can migrate it on KE02.

https://www.freescale.com/webapp/sps/download/preDownload.jsp

Xi

0 件の賞賛
返信
3,437件の閲覧回数
fantasy
NXP Employee
NXP Employee

HI, juan

I'd like to suggest you can choose the KE02 , KE02 is a 5 V MCU with enhanced FlexTimer(FTM), suitable for BLDC motor control. You can learn more detail information about KE02 through the link as below.

http://cache.freescale.com/files/32bit/doc/ref_manual/MKE02Z64M20SF0RM.pdf?fasp=1&WT_TYPE=Reference%...

And there is a ready-made solution to diver BLDC with FRDM-KE02Z. You can learn more about the solution by click the link below.

http://cache.freescale.com/files/32bit/doc/app_note/AN4776.pdf?fromsite

Have a good day,

Xi Fan

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,436件の閲覧回数
juanramonet
Contributor I

Hello,

I have one last question, on the ready-made solution for the motor control does the software used to control the motor have to be a CodeWarrior version, or are there any other softwares that could be used instead?

Thank you,

Juan

0 件の賞賛
返信
3,436件の閲覧回数
juanramonet
Contributor I

Thank you for the response, that was very helpful!

0 件の賞賛
返信