Yes, I tried that, no pull up is happening: Here are the relevant register settings.


Both outputs are configured as inputs, as you can see above (PDD = 0, right?)
One input is sitting at 0.2v the other is at .06. Interestingly, I can't pull them up with a 4700ohm resistor. Am I missing a setting somewhere? It's acting like they are set as outputs.
So, I tried to change the pin to an output, and write a 1, I also don't get any change
I set PDD= 0x00300000
and PDO= 0x00300000
both pins are still the same. Either I'm doing something wrong, or those inputs are damaged. Thanks for the help.
Geoff