Does anyone have example code for KE02Z ADC initialization?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anyone have example code for KE02Z ADC initialization?

3,192 Views
gmgjeg
Contributor II

Does anyone have example code for KE02Z  ADC initialization?  

0 Kudos
Reply
5 Replies

3,101 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bill Parks,

   You also can try the official KE02 sample code, which can be downloaded from this link:

https://www.nxp.com/webapp/Download?colCode=FRDM-KEXX-Driver-Library-Package&appType=license 

 ADC project folder:FRDM-KEXX-Driver-Library-Package\ke_drv_lib\build\iar\ke02\ADC_Poll_demo

Wish it helps you!

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,101 Views
gmgjeg
Contributor II

Thank you for your help, I really appreciate this.

On Thursday, December 27, 2018, 4:46:04 AM EST, kerryzhou <[email protected]> wrote:

|

NXP Community

|

Re: Does anyone have example code for KE02Z  ADC initialization? 

reply from Kerry Zhou in Kinetis Microcontrollers - View the full discussion

Hi Bill Parks,

   You also can try the official KE02 sample code, which can be downloaded from this link:

https://www.nxp.com/webapp/Download?colCode=FRDM-KEXX-Driver-Library-Package&appType=license 

 ADC project folder:FRDM-KEXX-Driver-Library-Package\ke_drv_lib\build\iar\ke02\ADC_Poll_demo

 

Wish it helps you!

If you still have question about it, please kindly let me know.

 

Have a great day,

Kerry

 

0 Kudos
Reply

3,101 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bill Parks,

     You are welcome!

     If you still have question about it, please kindly let us know.

     If your question is solved, please help me to mark the correct answer, just to close this post, thank you!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,101 Views
mjbcswitzerland
Specialist V

Hi

You can get ADC code in the open source uTasker project on GitHub (its ADC driver adapts itself to the ADC controller in the KE parts or others). It also allows the ADC to be simulated and tested in Visual Studio.

The file containing the code is called "kinetis_ADC.h".

Regards

Mark

0 Kudos
Reply

3,101 Views
gmgjeg
Contributor II

Thank you for the help.

On Wednesday, December 26, 2018, 6:24:17 PM EST, mjbcswitzerland <[email protected]> wrote:

|

NXP Community

|

Re: Does anyone have example code for KE02Z  ADC initialization? 

reply from Mark Butcher in Kinetis Microcontrollers - View the full discussion

Hi

 

You can get ADC code in the open source uTasker project on GitHub (its ADC driver adapts itself to the ADC controller in the KE parts or others). It also allows the ADC to be simulated and tested in Visual Studio.

 

The file containing the code is called "kinetis_ADC.h".

 

Regards

 

Mark

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Kinetis Microcontrollers by email or at NXP Community

Following Re: Does anyone have example code for KE02Z  ADC initialization?  in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply