Does anyone have an example code to work with the Ethernet module in the FRDM K64F on KDS enviroment? Thanks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anyone have an example code to work with the Ethernet module in the FRDM K64F on KDS enviroment? Thanks

3,206 Views
carlosorozco
Contributor I

Does anyone have an example code to work with the Ethernet module in the FRDM K64F on KDS enviroment? Thanks

Labels (1)
0 Kudos
Reply
5 Replies

2,744 Views
mjbcswitzerland
Specialist V
0 Kudos
Reply

2,744 Views
carlosorozco
Contributor I

I did it, i couldn't see nothing that can help me

0 Kudos
Reply

2,744 Views
mjbcswitzerland
Specialist V

Hi Carlos

Here is a screen shot of the page with the details that you missed:

pastedImage_1.png

Plus

pastedImage_2.png

It contains Ethernet code for your board and also a VisualStudio simulator which allows testing the Ethernet module in real-time on your PC.

More details here: https://community.freescale.com/message/400458#400458

Regards

Mark

0 Kudos
Reply

2,744 Views
carlosorozco
Contributor I

Can you give me the password to unzip the uTaskerKinetisV1.4.6 please? i requested it but i haven't recived it. Thanks

0 Kudos
Reply

2,744 Views
mjbcswitzerland
Specialist V

Hi Carlos

V1.4.7 is available for download without password protection. It is a newer version than V1.4.6 and has more features and device support.

You should receive the password for all archives shortly, but you will only need it for retrieving older versions in case of the need to unwind versions (which you won't as a new user).

Regards

Mark

0 Kudos
Reply