Does NXP provide flash tool for KW36?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP provide flash tool for KW36?

1,403 Views
jictannu
Contributor III

Hi, I would like a flash tool for KW36 except J-Flash. In MBOOTFLTOOLUG.pdf, it said there is a  Kinetis Flash Tool in  SDK package but I could not find this tool in SDK_2.2.1_FRDM-KW36. 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,298 Views
nxf58904
NXP Employee
NXP Employee

Hi,

You can use a Kinetis Flash Tool in other's SDK package(K64 or etc). Kinetis Flash Tool is used for connecting to a bootloader .  There has some other flash tools ,like J-link command,also can be used to program flash.

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply