Does NXP have a microcontroller with gigabit ethernet?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does NXP have a microcontroller with gigabit ethernet?

4,496件の閲覧回数
rikardlarking
Contributor I

I need a device with following interfaces

1x Gigabit ethernet interface

1x CAN interface

2-4x RS232

1-2x SPI.

Possibility to have a bootloader (with ethernet)

Free development platform

Easy to implement a UDP-communication

Bonus:

mbed-support

ADC / DAC

SD-card

Best regards,

Rikard

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,788件の閲覧回数
miduo
NXP Employee
NXP Employee

Yes, you may consider the i.MX6 SX device :

It has 2x Gigabit Ethernet with AVB-2x 10/100/1000 Mbps Gigabit Ethernet

(MAC) controllers (MII, RGMII) and two Flexible Controller Area Network (FlexCAN), 1 Mbps each.  

6 of UARTs and 5 of SPI. See detail from below link:

i.MX 6SoloX Family of Applications Processors|NXP

0 件の賞賛
返信