Does MKL25Z128VLK4 support flash swap?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MKL25Z128VLK4 support flash swap?

Jump to solution
4,321 Views
tuowang
Contributor II

Hi everyone,

I have a Kinetis KL25Z evaluation board with MKL25Z128VLK4. Does this MCU support flash swap feature?

Thanks

Tuo

0 Kudos
Reply
1 Solution
4,081 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tuo Wang:

KL25 MCU only contains 1 flash block, and it does not support flash swap functionality. For firmware update purposes (e.g. bootloader), the flash programming routines need to be run from RAM memory.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
4,082 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tuo Wang:

KL25 MCU only contains 1 flash block, and it does not support flash swap functionality. For firmware update purposes (e.g. bootloader), the flash programming routines need to be run from RAM memory.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,828 Views
gamine99
Contributor I

Hello Jorge,

We are currently using an MK60DN512, but due to its difficulty to source, we are considering using the MK60DN256ZVLL10 and urgently need to know if the flash swap feature is supported in the DN256 as this is critical to our application.

Also, do you know what the "Z" refers to and what Errata may exist for that part (DC 2019+).

Thank you!

0 Kudos
Reply
4,081 Views
tuowang
Contributor II

Thank you, Jorge! That's very helpful. Can you advise if there is any L series MCU that supports flash swap? Thanks Tuo

0 Kudos
Reply
4,081 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

You are welcome.

Unfortunately none of the L series support flash swap.

Regards!

Jorge Gonzalez

0 Kudos
Reply
4,081 Views
tuowang
Contributor II

Thank you Jorge!

0 Kudos
Reply