Does MK64F support Code Read Protection (CRP)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does MK64F support Code Read Protection (CRP)?

1,309件の閲覧回数
chhsu0229
Contributor II

I am working on Code Read Protection (CRP) with MK64F512x.

I now LPC MCU support CRP, however, MK64F support CRP, too?

Because I try to write Program Flash address 0x2FC and value is 0x12345678 (CRP_1).

It seems CRP does not work.

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,288件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

CRP is not supported in Kinetis families, this is from LPC MCUs only. For equivalent features, please check this application note.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 件の賞賛
返信