Does LCD 4bits/pixel TFT(480*272) mode of K70 work?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does LCD 4bits/pixel TFT(480*272) mode of K70 work?

1,015 次查看
applefly
Contributor II

I am trying to active the following LCD,

   1. use 4 bits per pixel TFT mode

   2. RAM buffer is set to 0x20000000 (SRAM_U start address)

   3. Per K70 datasheet, the total RAM buffer for LCD is 4 bits * 272* 480 = 64KByte.

       So I use all the SRAM_U(64K) as the RAM buffer.

My question are,

   1. I didn't find any limitation of this configuration in document, but this configuration can work?

   2.  I set relative configuration in LCDC registers, but it seems not works.

        I fill all the SRAM_U buffer to ZERO, but only 1/6(1/8) LCD pannel displays color...

         The other 5/6 keeps the same condition.


Thanks for  help!


Regards,

Mark

0 项奖励
回复
1 回复

858 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Mark,

  If you are using 4bpp TFT, then you must use the mapping RAM. See section 62.6.1 for details. Basically you need to put a sixteen 18-bit entries into the Background Look Up Table (BGLUT) to select which of the sixteen of the possible 256K colors to use. But yes, it does work.

  Here's some code specific for setting up the BGLUT that can get you started:

//Fill all 256 entries of the BackGround Look Up Table

//You would only need 16 for 4bpp mode

  for(i=0; i < 256; i++)

  {

    LUT_BG = (unsigned int *)0x400b6800 + i; //address in BGLUT

    *LUT_BG = 0x443322CC; //color value

  }

  printf("\nBackground Plane Lookup Table Filled\n");  

 

 

 

  printf("4bpp\n"); 

  SIM_MCR&=~SIM_MCR_LCDSTART_MASK;  //Stop LCDC 

  // set LCD panel configuration

  LCDC_LPCR =

    LCDC_LPCR_TFT_MASK      |       //TFT Screen

    LCDC_LPCR_COLOR_MASK    |       //Color

    LCDC_LPCR_BPIX(0x2)     |       //4 bpp

    LCDC_LPCR_FLMPOL_MASK   |       //first line marker active low

    LCDC_LPCR_LPPOL_MASK    |       //line pulse active low

    LCDC_LPCR_END_SEL_MASK  |     

    LCDC_LPCR_SCLKIDLE_MASK |       //Enalbe LSCLK when vsync is idle

    LCDC_LPCR_SCLKSEL_MASK  |       //Always enable clock

    LCDC_LPCR_PCD(0x3);             //Divide 120 PLL clock by (3+1)=4 to get 30MHz clock 

  SIM_MCR|=SIM_MCR_LCDSTART_MASK;  //Start LCDC   

-Anthony

0 项奖励
回复