Does K66 SDRAM controller support mobile low power SDRAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does K66 SDRAM controller support mobile low power SDRAM?

1,674 Views
paulakers
Contributor I

I am using the K66 (MK66FN2M0VMD18) and I am looking at adding some external SDRAM just in case we need more RAM area. Does the SDRAM controller support only SDRAM @ 3.3V or can it also support lpSDRAM (Micron’s Mobile low power SDRAM) @ 1.8V? For example this Micron P/N MT48H16M32LFB5-75 IT.

The K66 data sheet and reference seems to indicate only SDRAM and does not mention lpSDRAM support. In our case we are running the K66 only at 1.8V and if the K66 only supports SDRAM @ 3.3V, are we precluded from using any external SDRAM? (and we can’t add a bunch of level shifter buffers to support the 3.3V SDRAM).

Labels (1)
0 Kudos
Reply
1 Reply

1,505 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Paul

Unfortunately the k66 can not support LPSDR SDRAM

Have a good day.

0 Kudos
Reply