Does Developer's serial bootloader supports KE-02Z microcontrollers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Developer's serial bootloader supports KE-02Z microcontrollers?

Jump to solution
1,561 Views
ganeshramachand
Contributor IV

The application notes of Developer's Serial Bootloader in AN2295 states, "The microcontrollers supported by the developer's serial boot loader include 8-bit families HC08 and HCS08, and 32-bit families, ColdFire and Kinetis. New Kinetis families include support for K and L series. "

I would like to know whether it supports Kinetis E series controller too ?

To be specific I am using MKE02Z64VLD2 controller.

0 Kudos
Reply
1 Solution
1,371 Views
mjbcswitzerland
Specialist V

Hi

The AN2295 developer's loader is supported on the KE02 in the uTasker project:

http://www.utasker.com/kinetis/FRDM-KE02Z.html

http://www.utasker.com/kinetis/FRDM-KE02Z40M.html

and http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Also the KBOOT, SREC and IHEX loader modes can be used on the KE02.

Regards

Mark

View solution in original post

0 Kudos
Reply
1 Reply
1,372 Views
mjbcswitzerland
Specialist V

Hi

The AN2295 developer's loader is supported on the KE02 in the uTasker project:

http://www.utasker.com/kinetis/FRDM-KE02Z.html

http://www.utasker.com/kinetis/FRDM-KE02Z40M.html

and http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Also the KBOOT, SREC and IHEX loader modes can be used on the KE02.

Regards

Mark

0 Kudos
Reply