Documentation of SRS and SSRS Registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Documentation of SRS and SSRS Registers

1,016 次查看
Keith4DSmith
Contributor V

In document K22P121M120SF7RM Rev 4 8/2016 is documentation for both SRS and SSRS registers in Reset Control, RCM, Chapter 13

In document K22P144M120SF5V2RM Rev. 5 March 2015 is documentation of the SRS registers in Reset Control Module, RCM, Chapter 14.

Does this mean that some K22s do not support SSRS registers or is this missing documentation?

标签 (1)
0 项奖励
回复
1 回复

927 次查看
mjbcswitzerland
Specialist V

Hi Keith

F5 and F7 (K22) devices are not the same - check carefully which of the documents is relevant for the exact part that you use.

If you compare carefully there are a number of differences (often SW incompatible) between the various K22 devices.

For example F7 parts (ones with 128k or 512k Flash without NVRAM) have different base addresses for ADC1, have an additional options register (SIM_OPT8), have some different peripheral clocking controls (SIM_SCGC1). Also they have HSRUN mode to operate above 80MHz, whereas the F5 parts can run at 120MHz without the HSRUN mode restrictions. Some parts use long word Flash programming and others use phrase programming (so need different Flash drivers).......

There are more and I think that there is a document somewhere listing all of the things that need to be taken into account.

Regards

Mark

0 项奖励
回复