Do i need reset MCG clock when exiting LLS mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do i need reset MCG clock when exiting LLS mode

ソリューションへジャンプ
3,729件の閲覧回数
haizhouli
Contributor III

Hello all,

I am working on Low power mode on Kinetis K21. Based on page 31 in AN4503, I got this:

If the MCG was in PEE when LLS mode was entered from Run mode, it will exit in PBE mode. Note that any module's clocks sourced from the PLL have been off in LLS. Upon wake-up, the frequency will be changed and therefore baud rates and timer counter time bases will change as well. The PLL is functioning but not engaged.

Does this mean I have to reset MCG again to switch it from PBE to PEE once it exits from LLS mode?  Or I just need wait a little bit for PLL and system will be automatically back to PEE mode?

Thanks!

Haizhou

ラベル(2)
1 解決策
3,398件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hi Haizhou Li,

according to the kinetis_50MHz_sc (Sample Code from Freescale), the procedure which PLL waits for entering PEE mode after waking up from the low power mode is described as following. Therefore the answer is the latter of your candidates.


(1) Check MCG is in PBE mode, if not then error.
  if (!(
         (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) == 0x2) &&
         (!(MCG_S & MCG_S_IREFST_MASK)) &&
         (MCG_S & MCG_S_PLLST_MASK) &&   
          (!(MCG_C2 & MCG_C2_LP_MASK))
  ))  {   return ERROR;   }


(2) Check the PLL state before transitioning to PEE mode, if not then error.
  for (i = 0 ; i < 2000 ; i++)
  {
    if (MCG_S & MCG_S_LOCK0_MASK) break;
  }
  if (!(MCG_S & MCG_S_LOCK0_MASK)) return ERROR;

(3) Clear CLKS to switch CLKS mux to select PLL as MCG_OUT.
  MCG_C1 &= ~MCG_C1_CLKS_MASK;

(4) Wait for clock status bits to update, if not then error.
  for (i = 0 ; i < 2000 ; i++)
  {
    if (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) == 0x3) break;
  }
  if (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x3) return ERROR;

I hope it will help you.

Best regards,
Yasuhiko Koumoto.

元の投稿で解決策を見る

5 返答(返信)
3,398件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi HaiZhou

When the MCG in PEE mode enter in LLS mode, it exits in PBE mode.

So, it need software to switch MCG working mode from PBE to PEE again.

K21 120MHz example code provides MCG module driver and includes pbe_pee() function.

More detailed info, please download K21 120MHz example code below:

http://cache.freescale.com/files/32bit/software_tools/TWR-K21F120M_LABTS.zip


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,398件の閲覧回数
haizhouli
Contributor III

Thanks very much for the help and link. Really appreciate!

0 件の賞賛
返信
3,399件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hi Haizhou Li,

according to the kinetis_50MHz_sc (Sample Code from Freescale), the procedure which PLL waits for entering PEE mode after waking up from the low power mode is described as following. Therefore the answer is the latter of your candidates.


(1) Check MCG is in PBE mode, if not then error.
  if (!(
         (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) == 0x2) &&
         (!(MCG_S & MCG_S_IREFST_MASK)) &&
         (MCG_S & MCG_S_PLLST_MASK) &&   
          (!(MCG_C2 & MCG_C2_LP_MASK))
  ))  {   return ERROR;   }


(2) Check the PLL state before transitioning to PEE mode, if not then error.
  for (i = 0 ; i < 2000 ; i++)
  {
    if (MCG_S & MCG_S_LOCK0_MASK) break;
  }
  if (!(MCG_S & MCG_S_LOCK0_MASK)) return ERROR;

(3) Clear CLKS to switch CLKS mux to select PLL as MCG_OUT.
  MCG_C1 &= ~MCG_C1_CLKS_MASK;

(4) Wait for clock status bits to update, if not then error.
  for (i = 0 ; i < 2000 ; i++)
  {
    if (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) == 0x3) break;
  }
  if (((MCG_S & MCG_S_CLKST_MASK) >> MCG_S_CLKST_SHIFT) != 0x3) return ERROR;

I hope it will help you.

Best regards,
Yasuhiko Koumoto.

3,398件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hi  Haizhou Li,

my descriptions are just the pbe_pee function contents. I checked the differences them from the sample code shown by Mr. Mui Ma. As the result it is identical.

Best regards.

Yasuhiko Koumoto.

0 件の賞賛
返信
3,398件の閲覧回数
haizhouli
Contributor III

thanks very much!

0 件の賞賛
返信