Do all KL03 GPIO pins have pullup / pulldown resistors available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do all KL03 GPIO pins have pullup / pulldown resistors available?

1,361 Views
thomasedel
Contributor III

I'm trying to determine which pins on the KL03 have pullup and pulldown resistors.  I can't find that information in the various documentation.  Does anyone know where that information is, or otherwise know the answer?  Thanks in advance for your help.

-Thomas

Labels (1)
0 Kudos
Reply
1 Reply

1,236 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Thomas:

Yes, all PTA/PTB pins of KL03 should have pull enable and pull select control. This information is in a table in the reference manual:

pastedImage_0.png

Best regards,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply