KL03 power required to run CMP and 6-bit DAC in standby mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL03 power required to run CMP and 6-bit DAC in standby mode?

1,098件の閲覧回数
thomasedel
Contributor III

I can't find any data regarding the power used by the KL03 comparator while in standby mode (when using the CMP and 6-bit DAC in trigger mode; while waiting to be triggered).  Some documents imply lower power than normal enabled-mode power, but I can't find any specifics. Some specs show the the normal enable-mode current to be about 15uA to 25uA (typical or maximum for low power mode), but I don't see any data for standby mode while waiting for a trigger. 

Thanks in advance for any help with this.

-Thomas

ラベル(1)
0 件の賞賛
返信
1 返信

956件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Thomas

I am not sure if this what you are looking for

pastedImage_0.png

Please check the table 11 in the data sheet

Regards

Vicente Gomez

0 件の賞賛
返信