Disabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disabled

1,879 Views
hisanoriterashi
Contributor I

The DAC output pin keeps "disabled" during RESET period, the Reference

manual says.

So I will supply some DC on the DAC pin to check and adjust the Analogue

circuit surrounding the MCU at very beginning of the development.

What does "disable" mean?

If it means uncontrol and HIGH IMPEDANCE, my method may acceptable.

If not, DC supply may cause any troubles on the MCU chip.

GIVE me a correct Answer please.

--

ECTE

Electronics Consultative Tera Engineering

寺嶋 久憲

[email protected]

090-9320-7601

[email protected]

0 Kudos
Reply
1 Reply

1,775 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Terashima-san

Yes, "disable" means that this pins are in high-impedance status. So I think your application can use this chip. Thanks.

Best Regards

Paul

0 Kudos
Reply