Disabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Disabled

1,891 次查看
hisanoriterashi
Contributor I

The DAC output pin keeps "disabled" during RESET period, the Reference

manual says.

So I will supply some DC on the DAC pin to check and adjust the Analogue

circuit surrounding the MCU at very beginning of the development.

What does "disable" mean?

If it means uncontrol and HIGH IMPEDANCE, my method may acceptable.

If not, DC supply may cause any troubles on the MCU chip.

GIVE me a correct Answer please.

--

ECTE

Electronics Consultative Tera Engineering

寺嶋 久憲

[email protected]

090-9320-7601

[email protected]

0 项奖励
回复
1 回复

1,787 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Terashima-san

Yes, "disable" means that this pins are in high-impedance status. So I think your application can use this chip. Thanks.

Best Regards

Paul

0 项奖励
回复