Differential 16 bit ADC CMRR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differential 16 bit ADC CMRR

Jump to solution
1,927 Views
PatrickD
Contributor II

Hi Everyone

I have spent some time trying to discover the common mode rejection ratio of the Kinetis K series internal ADC configured in 16 bit differential mode and have ploughed through datasheets, reference manuals and application notes without success. I have also performed web searches with similar results. CMRR is surely a salient parameter for any differential device and one would expect this to be clearly stated somewhere as without this detail it is practically impossible to estimate the degree of immunity to external interfering signals. Would anyone be party to this information?

Regards

Patrick

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,700 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Patrick,

In data sheet of Kinetis, we define the CMRR spec for AD, it is about 84dB, in other words, the effect is about 1/10000. I cut it from the data sheet of K60P144M120SF3.pdf.

BR

Xiangjun Rong

pastedImage_0.png

View solution in original post

0 Kudos
Reply
1 Reply
1,701 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Patrick,

In data sheet of Kinetis, we define the CMRR spec for AD, it is about 84dB, in other words, the effect is about 1/10000. I cut it from the data sheet of K60P144M120SF3.pdf.

BR

Xiangjun Rong

pastedImage_0.png

0 Kudos
Reply