Differences bewteen AWIC and WIC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences bewteen AWIC and WIC?

Jump to solution
4,229 Views
yasuhikokoumoto
Senior Contributor I

Hello experts,

does anyone tell me the differences between AWIC (Asynchronous Wake-up Interrupt Controller) and WIC (Wake-up Interrupt Controller)?

WIC is described in the ARM's reference manual as a part of CPU component.

However, there are not words of WIC in the Kinetis reference manuals. Instead there is AWIC.

Why it is not WIC but AWIC?

Or, those are the same?

Thank you and best regards,

Yasuhiko Koumoto.

Tags (1)
0 Kudos
Reply
1 Solution
3,511 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yasuhiko Koumoto,

They are not the same, the AWIC has the advantage that it can wake up the system without a clock.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
3,512 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yasuhiko Koumoto,

They are not the same, the AWIC has the advantage that it can wake up the system without a clock.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,511 Views
yasuhikokoumoto
Senior Contributor I

Hello Kan_Li,

thank you! AWIC is the original module of the freescale, isn't it?

Best regards,

Yasuhiko Koumoto.

0 Kudos
Reply
3,512 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yasuhiko Koumoto,

Yes, it is.


Have a great day,
Kan

0 Kudos
Reply