Differences bewteen AWIC and WIC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Differences bewteen AWIC and WIC?

跳至解决方案
4,233 次查看
yasuhikokoumoto
Senior Contributor I

Hello experts,

does anyone tell me the differences between AWIC (Asynchronous Wake-up Interrupt Controller) and WIC (Wake-up Interrupt Controller)?

WIC is described in the ARM's reference manual as a part of CPU component.

However, there are not words of WIC in the Kinetis reference manuals. Instead there is AWIC.

Why it is not WIC but AWIC?

Or, those are the same?

Thank you and best regards,

Yasuhiko Koumoto.

标记 (1)
0 项奖励
回复
1 解答
3,515 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yasuhiko Koumoto,

They are not the same, the AWIC has the advantage that it can wake up the system without a clock.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,516 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yasuhiko Koumoto,

They are not the same, the AWIC has the advantage that it can wake up the system without a clock.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,515 次查看
yasuhikokoumoto
Senior Contributor I

Hello Kan_Li,

thank you! AWIC is the original module of the freescale, isn't it?

Best regards,

Yasuhiko Koumoto.

0 项奖励
回复
3,516 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Yasuhiko Koumoto,

Yes, it is.


Have a great day,
Kan

0 项奖励
回复