Difference between CodeWaarrior and Kinetis Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between CodeWaarrior and Kinetis Design Studio

9,537件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

     I want to know the difference between CodeWarrior and Kinetis Design Studio ?

Please give me a detailed information about the pros and cons between both of them.Please provide me the screen shots of the pros and cons also.

20 返答(返信)

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Thank you Erich It gave me a lot of insights. I want to import a code Warrior project to KDS and I encountered this error

Screenshot (19).png

Can you tell me the reasn for it?

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I general, I recommend to create a new project with the wizard and then add your source files to it. Much easier, simpler and usually the way to go.

As for that error, see the description about it in Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V...

I hope this helps,

Erich

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             Ya that is the way to go by creating a new project and importing source files but i want to know the reason why i am not able to build eventhough i followed the same steps as in the above discussion link given by you and I also followed a document for importing a codeWarrior project into KDS.This is the link for that document http://cache.nxp.com/files/microcontrollers/doc/user_guide/KDSPUG.pdf?fpsp=1&WT_TYPE=Users%20Guides&...

I want to understand the problem and things behind it instead of just considering it as a black box.I got an error message saying "ld returned 1 exit status"

which should go off if I include librt as per the document but it didn't can you help me out in finding the reason and solution for it.

Screenshot (22).png

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Vignesh,

see the same document Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V... about semihosting. I think you have not set the no-sys option?

Erich

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             My project is build but I am not able to run it.The error log showed these messages.

Screenshot (24).png

Can you help  me the reason for it and how to fix it?

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The 'orphaned' messages in your problem view are telling me that you are not using a KDS project (maybe you are using a CodeWarrior project, or from the message as well a CodeSourcery project).

Please make sure your project is a KDS project.

I hope this helps,

Erich

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             It is Actually an Imported Project from CodeWarrior.Can you say me what I missed or what should be done to fix it?

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Importing (with File > Import > Existing Project) does not convert the project. I recommend that you create a new project with File > New Kinetis Project for your device and then add your source files to that project.

Erich

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             I followed your same steps by crating a new kds project and copy pasting the same source files but I got an error like this while building.

Screenshot (26).png

Eventhough the commom.h file is there it is throwing an error like this???

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You need to specify the directories where the compiler can find the header files, like in the example below:

include.jpg

Erich

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             I did the changes suggested by you.Now I am able to build the project but I am not able to Run or Debug it.It shows me these error messages.

Screenshot (30).png

Screenshot (29).png

It is throwing me an error message like this.How to fix this???

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

I suggest to follow the advice in that dialog box.

Erich

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

     Hi Erich,

                   I fixed that problem.The cable was causing it.But now I am able to comfortably bebug or flash in CodeWarrior but not in KDS.It is showing a dialog like this.

Screenshot (31).png

Can you tell me how to fix it???

0 件の賞賛
返信

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             I checked the connection.It is proper.I am able to Flash code From CodeWarrior with the same connection???

0 件の賞賛
返信

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Does nanolibc include va_list in it ???

0 件の賞賛
返信

8,279件の閲覧回数
BlackNight
NXP Employee
NXP Employee

No sure if I understand. But the nano-lib includes the standard C libraries which support variable arguemnt lists.

Erich

0 件の賞賛
返信

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Thank you Erich,

                           I am able to build it now.I added the new library nanolib using --specs=nano.specs and then I added the semihosting -specs=rdimon.specs.I have attached the screenshot of it.

Screenshot (23).png

0 件の賞賛
返信

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Please tell me where to add the Linker options???

0 件の賞賛
返信

8,279件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Erich,

             I got to know that it is because of semi-hosting.where to give the instruction -specs=rdimon.specs.Please tell me where to make changes to execute semi-hosting?

0 件の賞賛
返信