Detection distance USB ZigBee Packet Sniffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Detection distance USB ZigBee Packet Sniffer

1,817 Views
k_vanderheiden
Contributor I

I am about to use the USB-KW24D512 as a ZigBee packet sniffer. Can someone tell me (theoretically or by experience) what would be max distance the sniffer will detect packets? (Indoor and outdoor)

Thanks!

0 Kudos
Reply
2 Replies

1,665 Views
AngelC
Senior Contributor I

Dear K. van der Heiden,

The sniffer itself has a RX sensitivity of around –100 dBm, so it could still receive signals of such energy level. However, the maximum distance would depend more in the devices transmitting and the output power they are capable to achieve.

Between two USB-KW24D512 boards you will be able to transmit and receive within 30 meters indoors approximately. However, if another device (bigger antenna, printed antenna, power amplifier, etc.) has the ability to transmit to a long distance (i.e. TWRKW2x boards could achieve around +8dBm), the sniffer would still detect the packets from tens to hundreds of meters.

In brief, as long as the transmitted signal has enough energy, it will be detected and received by the USB-KW24D512.

Regards,

AngelC

1,665 Views
k_vanderheiden
Contributor I

Ok, this information is what I need for now. Thanks for you reply, AngleC!

0 Kudos
Reply