Demo code for using EEPROM feature on K20, 50 Mhz device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Demo code for using EEPROM feature on K20, 50 Mhz device

2,875 Views
ajaybharti
Contributor I

Does any one having demo code for EEPROM functionality on K20, 50Mhz device using with or without PE support.

Labels (1)
0 Kudos
Reply
3 Replies

2,292 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ajay Bharti,

     The attached is my K20 50Mhz code, This the EPPROM function, I write this code based on hello world.

     You can use it directly, I already test it base on K20D50M tower board.

     Wish it helps you!

Best regards!

Jingjing

0 Kudos
Reply

2,290 Views
perlam_i_au
Senior Contributor I

I suggest you to review the application note AN4282 Using the Kinetis Family Enhanced EEPROM Functionality, I hope you find it useful.

0 Kudos
Reply

2,290 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ajay Bharti,

     About the EEPROM code of K 20 50Mhz, actually, in our www.freescale.com, there has a flash driver which include this code, please download the driver from this link:

     http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fromsite=zh-Hans&Parent_node...

     After the soft setup in default, you will find the code in the path:C:\Program Files\Freescale\Standard Software Driver vBeta035\C90TFS\Demos\build

     This code is base on the APIs function, and in the soft setup root directory, there has a document named of UM_C90TFS_FTFx_SSD.pdf, it describes the function in details.

     I wish my answer will help you!

    If you still have question, please contact with me!

Best regards!

Jingjing

0 Kudos
Reply