Default Core Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Default Core Clock

2,381 Views
mithunp_s
Contributor III

Hi All,

I'm using PT60 & FRDM board,

Once I create a bare board project in CW for any of these device (S08, KL) I want to know what will be default Core Clock codewarrior sets.

I know how to set particular clock frequency in both PE & nonPE projects,  but I want to know in bare board project what will be default setting once project is created, where can find these settings in project and can I directly modify these settings as per my requirement.

Rgds

Mithun

0 Kudos
Reply
4 Replies

2,189 Views
JimDon
Senior Contributor III

Also, if you use PE to set the clocks, you can see exactly what the clocks will be and how to set it there.

0 Kudos
Reply

2,189 Views
adriansc
Contributor IV

Hi,

For KL CW does not code this configuration, MCG comes out the reset in FEI (FLL Engaged Internal) mode (as Jim Donelson said) and you need to add code in order to change MCG modes. Check MCG mode state diagram:

Default core clock 1.png

It applies the same for S08 device: FEI is the default mode of operation for ICS; and CW does not code it.

Default core clock 2.png

Hope this helps.

0 Kudos
Reply

2,189 Views
Monica
Senior Contributor III

Mithun, how is it going?

Please keep us posted :smileywink:

Monica

0 Kudos
Reply

2,189 Views
JimDon
Senior Contributor III

>in bare board project what will be default setting once project is created, where can find these settings in project and can I directly modify these settings as per my requirement.

There are no settings for the clock (or anything else like that) in a bare board project. You need to add code for this.

This may apply to all Kinetis chips:

25.5.2 Using a 32.768 kHz Reference

"In FEE and FBE modes, if using a 32.768 kHz external reference, at the default FLL

multiplication factor of 640, the DCO output (MCGFLLCLK) frequency is 20.97 MHz at

low-range."

0 Kudos
Reply