Dedicated Pins in MK22FN512VLL12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dedicated Pins in MK22FN512VLL12

1,397 Views
prasannanaik
Contributor III

Hi,

   I am using MK22FN512VLL12 in a control application where i have a lot of interfaces. I am facing shortage of GPIOs. While going through datasheet, i found that the following pins are dedicated for single purpose only ( They can't be used as even GPIOs)

Sr. no

PIN no

Description

1

10

USB0_DP

2

11

USB0_DM

3

12

VOUT33

4

13

VREGIN

5

14

ADC0_ DP1

6

15

ADC0_ DM1

7

16

ADC1_ DP1/ ADC0_ DP2

8

17

ADC1_ DM1/ ADC0_ DM2

9

18

ADC0_ DP0/ ADC1_ DP3

10

19

ADC0_ DM0/ ADC1_ DM3

11

20

ADC1_ DP0/ ADC0_ DP3

12

21

ADC1_ DM0/ ADC0_ DM3

 

Please help in resolving following queries:

1) Can ADC DP/DM lines be used for single ended analog measurement?

2) Can all/any of these pins be used as GPIOs?

Thanks and best regards,

Prasanna

Labels (1)
1 Reply

1,316 Views
mjbcswitzerland
Specialist V

Hi

The ADC inputs with "P" and "M" can be used either as single ended inputs or, when paired, as differential inputs to a single channel.

None of these pins can be used as GPIO since they are dedicated to their analogue functions.

Regards

Mark

Complete Kinetis solutions for professional needs, training and support: http://www.utasker.com/kinetis.html
Kinetis K22:
- http://www.utasker.com/kinetis/FRDM-K22F.html
- http://www.utasker.com/kinetis/TWR-K22F120M.html
- http://www.utasker.com/kinetis/BLAZE_K22.html
- http://www.utasker.com/kinetis/tinyK22.html

uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market
Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis