Decimal value of 0x1M?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Decimal value of 0x1M?

1,381件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    I want to know the decimal value of 0x1M???

Is 0x1M - 0x1800  = 0x000FF000  ???

ラベル(2)
3 返答(返信)

1,274件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Before answer your question, I was wondering if you can share the total codes.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,273件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    I am trying to understand this document which I have attached in the thread.I want to understand listing 10 in it, How my_text section gets it's start address and is it from m_text origin plus length of m_text which will give my_text start address????

0 件の賞賛
返信

1,273件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

The 0x1M means 0xFFFFF, and the range of the my_text segment is from the 0x000FF000 to 0x000FFFFF.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信