Debugger PE Micro connection error for S32K396

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger PE Micro connection error for S32K396

ソリューションへジャンプ
2,742件の閲覧回数
Silvano
Contributor I

Hi,

 

I have this error when I try to debug the S32K396-LQFP-DC : 

Silvano_0-1709134668919.pngSilvano_1-1709134700046.png

Silvano_2-1709134717849.png

 

This is how I connect the board : 

20240228_163038.jpg

 

Could you help me please ?

Thank you.

タグ(1)
0 件の賞賛
返信
1 解決策
2,668件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

LQFP is supported in RTD 4.0.0. You should see this version in the Standard Software package:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

Regards,

Lukas

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,706件の閲覧回数
Silvano
Contributor I

I finally succeed to communicate with the board, thank you. I have a last question, where can I find the coorect package for the S32K396-LQFP-DC ? Because I have only package for the S32K396_289bga-BGA 289 package. So when I try to compute the code example " Blinking led" , I can not see the led blinking. 

Silvano_0-1709307654651.pngSilvano_1-1709307943339.png

Silvano_2-1709308024259.png

 

 

0 件の賞賛
返信
2,669件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

LQFP is supported in RTD 4.0.0. You should see this version in the Standard Software package:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D

Regards,

Lukas

 

0 件の賞賛
返信
2,711件の閲覧回数
Silvano
Contributor I

Hi @lukaszadrapa 

Where may I find the schematic that you use in your message ? I have the spf-54614_a.pdf version.

Also, which jumper configuration do you suggest for in-built OpenSDA interface ?

0 件の賞賛
返信
2,717件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Silvano 

if you use in-built OpenSDA interface, you need to select it by jumpers. I can see that ARM connector is selected now:

lukaszadrapa_0-1709286654899.png

 

Regards.

Lukas

0 件の賞賛
返信