Debouncing time in TSS3.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debouncing time in TSS3.1

ソリューションへジャンプ
1,946件の閲覧回数
sureshjaggal
Contributor III

Dear Folks,

I am using TSS3.1 in TSI configuration and KL05Z32 to develop a HMI application.

It is mentioned in the TSS application reference manual that the debouncing time  for the touch Input is taken care by the TSS library .

My questions are

1) How much is the debouncing time , that the TSS is configured with ?

2) How can we change the debouncing time for our requirements in TSS ?

Thanks & Regards,

Suresh Jaggal. 

ラベル(2)
タグ(2)
1 解決策
1,866件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Suresh

The debouncing rate is modified with the ResponseTime register that defines how many samples need to be valid before considering a measured value as valid. The feature is available in all key detector versions. Refer to the TSS reference manual - Number of samples register.

Depending your application maybe you need more or less samples for your application.

I hoe this will help you.

Regards

Vicente.

元の投稿で解決策を見る

1 返信
1,867件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Suresh

The debouncing rate is modified with the ResponseTime register that defines how many samples need to be valid before considering a measured value as valid. The feature is available in all key detector versions. Refer to the TSS reference manual - Number of samples register.

Depending your application maybe you need more or less samples for your application.

I hoe this will help you.

Regards

Vicente.