Dear engineers FREESCALE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dear engineers FREESCALE

2,883 次查看
Microfelix
Contributor IV

Dear engineers FREESCALE.

They are about 3 years to work with your Kinetis series processors.

For accuracy, the K60 and then K70.

And 'more than a year that feels around rumors regarding a possible X-series, which has superior performance to the K70.

The competitor has made ​​MICROCHIP PIC32 microprocessor series up to 2M of internal flash memory.

FREESCALE expect the thing to develop a series of Kinetis processor with more memory? We have news of a possible way out?

Maurizio Felicioni

标记 (1)
0 项奖励
回复
5 回复数

2,368 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Maurizio

Up to now, Kinetis X series is still in process. We have a plan for bigger size flash chip in Kinetis family.

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复

2,368 次查看
Microfelix
Contributor IV

I would like to have a date, 2014, 2015?

Thanks Maurizio

0 项奖励
回复

2,368 次查看
GregC
NXP Employee
NXP Employee

Hi Maurizio

Kinetis K64 and K24 have been released this summer with 256KB RAM and up to 1MB of Flash based on an ARM Cortex-M4 core @120MHz with FPU and new features like Crystal-less USB or lower-power capabilities.

End of 2014 new Kinetis K6x derivatives extending the K64 should be available embedding more flash and with a significantly higher core frequency.

Regarding the availability of Kinetis-X, even if there is no official message, a full-production in 2015 seems more reasonable.


Did I answer well your question ?

Greg

0 项奖励
回复

2,368 次查看
Microfelix
Contributor IV

hello

now we got to the end of 2014.

But still no sign of new products.

Any news?

Maurizio

0 项奖励
回复

2,368 次查看
Microfelix
Contributor IV

Dear Greg,

thanks for your reply.

I hope that the freescale releases a K70 with more than 1M of flash memory.

Maurizio

0 项奖励
回复