Daplink firmware compatibility with K64 device family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Daplink firmware compatibility with K64 device family

4,911件の閲覧回数
Asad_Khan
Contributor II

Hi,

I have designed a custom board using NXP MK64FX512 MCU and included the OpenSDA circuit from the FRDM-K64F board.
For OpenSDA, I have flashed the latest FRDM-K64F DAPlink bootloader and target firmware interface files, as mentioned on the daplink.io website.

After flashing the bootloader file, I am able to copy and paste the firmware interface file on Mk20 MCU, but while debugging on MCUXpresso it is giving me the error:>
" Unable to connect wire for probe index 1" Error: Wire Ack Fault - target connected?

I also checked the hardware, everything looks ok and there is no issue with the hardware.

So, I just want to confirm whether the FRDM-K64F Daplink bootloader and firmware interface files will work with target MCU MK64FX512xx or not! The bootloader and firmware interface files are device specific? Because the FRDM-K64F board has a different target device MK64FN1Mxx.

Thanks,
Mohammad Asad Khan

 

0 件の賞賛
返信
7 返答(返信)

4,902件の閲覧回数
ErichStyger
Specialist I

The 'copy and paste' part depends on the target MCU, so is specific, because it needs to know about the memory map and flash algos.

The debugging part itself does not (or should not) depend on the OpenSDA firmware, as this knowledge is on the host/debugger side.

Were you able to debug initially? I think with your drag&drop you screwed up the target, so it constantly resets, and the OpenSDA K20 is not able to take over control.

Do you still have a debug header? If so, you could try this: https://mcuoneclipse.com/2021/05/20/recovering-cortex-m-microcontroller-with-a-power-glitch/

I hope this helps,

Erich

0 件の賞賛
返信

4,895件の閲覧回数
Asad_Khan
Contributor II
Hi Erich,
I have downloaded the firmware files from this link.

https://www.nxp.com/design/software/development-software/sensor-toolbox-sensor-development-ecosystem...

Thanks,
Mohammad Asad Khan
0 件の賞賛
返信

4,892件の閲覧回数
ErichStyger
Specialist I

What firmware are you using?

Keep in mind that the P&E and SEGGER firmware do not allow you to use it with your custom hardware. You would have to use the ARM DAPLink one: https://github.com/ARMmbed/DAPLink

 

0 件の賞賛
返信

4,890件の閲覧回数
Asad_Khan
Contributor II
Yes, I am using the DAPlink firmware only. But it is not mentioned anywhere whether it will support K64 family devices or it is a single device-specific firmware.
0 件の賞賛
返信

4,886件の閲覧回数
ErichStyger
Specialist I

So here is how I can use the DAPLink bootloader and firmware with my K22FX:

- using v0257 from https://github.com/ARMmbed/DAPLink/releases

- programmed 0257_k20dx__0x0000.bin at address 0x0

- programmed 0257_k20dx_frdmk20dx_0x8000.bin at address 0x8000

- debugging my application using MCUXpresso IDE 11.6.0, the DAPLink gets recognized as LinkServer connection

Note:

- I'm not using the MSD Drag&Drop programming, so I don't care that the firmware is for K20

- I'm not actively using the DAPLink because it is so slow. But if you have nothing else available, it is better than nothing

 

I hope this helps,

Erich

0 件の賞賛
返信

4,897件の閲覧回数
Asad_Khan
Contributor II
Hi Erich,

Thanks for the reply.
So, it means the FRDM-K64F OpenSDA firmware interface will work only with its target device (MK64FN1Mxx) and for all K64F family devices.

If I connect the external debugger with the target MCU then I can able to debug. In my case, the external debugger is Multilink universal from PEmicro.
Thanks,
Mohammad Asad Khan
0 件の賞賛
返信

4,896件の閲覧回数
ErichStyger
Specialist I

it all depends what you use as 'firmware' on top of the MSD bootloader: if that firmware is device specific, then it only works for that given device.

0 件の賞賛
返信