DVP & Flex Bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,238件の閲覧回数
josephchen
Contributor III

Is Digital Video Port interface same as Flex Bus interface?

Can I use K series MCUs to connect to camera module via Digital Video Port interface?

ラベル(1)
1 解決策
3,961件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joseph Chen,

I have looked into the data sheet of OV9712, but found its interface is different from flexbus signals, so I think this DVP interface can not be connected with flexbus, while the GPIO solution should be ok.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

7 返答(返信)
3,961件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joseph,

Which DVP product you are referring to? FlexBus might fit with some of them but not all in the world. Would you please help to provide more details? Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,961件の閲覧回数
josephchen
Contributor III
0 件の賞賛
返信
3,961件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Joseph,

Please review the following appnote to see if it will help.

AN4627, Connecting Kinetis MCU with CMOS Sensor Interface through GPIO - App ... (REV 0)

30 May 2013 AN4627: This application note explains how to connect a Kinetis MCU to CMOS  Sensor through GPIO to receive image data in memory. ...
  • PDF 
  • 77KB  
  • Application Notes: AN4627
Associated File: AN4627SW

Regards,

David

0 件の賞賛
返信
3,961件の閲覧回数
josephchen
Contributor III

I've researched on the appnote, but it's talking about connecting via GPIO instead of Flex Bus. Also, I'm still not sure whether DVP output can be connected via Flex Bus or not.

0 件の賞賛
返信
3,962件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Joseph Chen,

I have looked into the data sheet of OV9712, but found its interface is different from flexbus signals, so I think this DVP interface can not be connected with flexbus, while the GPIO solution should be ok.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,961件の閲覧回数
DavidS
NXP Employee
NXP Employee

Thank you Kan for looking into the details.

Very much appreciated.

Regards,

David

0 件の賞賛
返信
3,961件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Joseph,

Just wanted to point that AppNote out to you and others and to say it has been implemented by more than one customer successfully.

Regards,

David

0 件の賞賛
返信