DTCM/ITCM Aliasing? (KV5X)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DTCM/ITCM Aliasing? (KV5X)

Jump to solution
1,767 Views
lsrbigfoot
Contributor IV

While using the K20/K22 (cortex-M4), I have been using bit-banding macros to access the aliased region for SRAM_U (0x20000000 to 0x2000FFFF).

Example Macro:
#define BandAddr 0x22000000
#define BitBandMem(Addr, Bit)     (*(volatile uint32_t*)(BandAddr + ((((uint32_t)Addr) & 0x3FF) << 5) + (((uint8_t)Bit) << 2)))

Does the KV5X (Cortex-M7) support bit-banding to both ITCM and DTCM memories (D0TCM and D1TCM) if I were to use similar macros?

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,572 Views
chris_brown
NXP Employee
NXP Employee

Hi lsrbigfoot,

So not natively.  There is no aliased region for the ITCM or DTCM areas to write to.  

But we did implement the BME2 engine for just such a request.  You should be able to find the necessary information in chapter 24 of the KV5x reference manual, as well as some examples.  Please let me know if you have further questions about that. 

Best regards,

Chris 

View solution in original post

1 Reply
1,573 Views
chris_brown
NXP Employee
NXP Employee

Hi lsrbigfoot,

So not natively.  There is no aliased region for the ITCM or DTCM areas to write to.  

But we did implement the BME2 engine for just such a request.  You should be able to find the necessary information in chapter 24 of the KV5x reference manual, as well as some examples.  Please let me know if you have further questions about that. 

Best regards,

Chris