DMAMUX MKV58

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMAMUX MKV58

2,814件の閲覧回数
jmasgiro
Contributor I

Can I configure DMAMUX with CH0 routed with source 16 (SPI0 Receive) and CH17 routed with source 16 (SPI1 Receive)? According to the KV58F2M0VLQ24 datasheet, on DMAMUX chapter, source 16 has a different peripheral associated with it depending on whether you use the 0-15 or 16-31 channels.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,778件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

Unfortunately, this is not possible, because the source is the same and only changes according to the output channel.

Best regards,
Pavel

 

0 件の賞賛
返信

2,775件の閲覧回数
jmasgiro
Contributor I

Dear Pavel_Hernandez, 

thank you very much for your advice. The only solution I have is use SPI2 instead of SPI1.

Best regards

2,781件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Let me review your information, when I have more details I will contact you.

Best regards,
Pavel

0 件の賞賛
返信